Technical FAQs

Ask a Question

Does Square D/SE offer a CSED All-In-One, same as the SC1624M100F but rated for 22k SCCR?

Product Design features

Product Line:
Combination Service Entrance Devices

Short circuit current rating


NO, Square D does not offer a CSED All-In-One same as the SC1624M100F rated for 22,000 SCCR. However, we do have a 20 space/40 circuit, 125 ampere device that you may consider, catalog number SC2040M125PF. This device uses the QOM2125VH Main Breaker and is rated 22,000 AIC. For overhead service, a SCTKP20 Tunnel Kit would be required.

CTA-ID : 15640
Was this helpful?
What can we do to improve the information ?