Technical FAQs

Ask a Question

What is part number for a 9001 Type K 3 position maintained selector switch for a HOA application, with the following contact sequence: O O X , X O O?

Issue:
What is part number for a 9001 Type K 3 position maintained selector switch for a HOA application, with the following contact sequence:

O O X
X O O

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product selection

Resolution:
9001KS43BH13.


CTA-ID : 15363
Was this helpful?
What can we do to improve the information ?