Technical FAQs

Ask a Question

What Tenant Circuit Breakers can be used with a EZM315125 Meter Center?

Issue:
Product Design Features

Product Line:
EZ Metering Equipment

Environment:
Tenant breakers

Cause:
Application/Installation

Resolution:
This EZM Meter Center uses QO, QO-VH or QOH, 125 ampere Maximum, tenant circuit breakers. Example Catalog Number for 125 ampere - QO2125, QO2125VH or QOH2125.


CTA-ID : 15902
Was this helpful?
What can we do to improve the information ?