Technical FAQs

Ask a Question

What is the Terminal Lug Data for the old 92444 Double Throw Safety Switch?

Issue:
Product design features

Product Line:
Double Throw Safety Switches

Environment:
wire size

Cause:
installation

Resolution:
The lugs on this device will accept (1) #6 AWG - 300 kcmil Aluminum or Copper conductors per phase.

 
Was this helpful?
What can we do to improve the information ?