Technical FAQs

Ask a Question

Does a QO260NATS include a neutral?

No, a neutral assembly is not supplied. A ground bar kit is included. The device is suitable for 240 Vac loads only. For a 120/240 Vac application, consider a QO2000NS.


CTA-ID : 15348
Was this helpful?
What can we do to improve the information ?