Technical FAQs

Ask a Question

Does the load center included in a HOMVP9 Value Pack accept tandem breakers?

Product Features

Product Line:
Homeline LC

Clarification of product design feature

Yes, the HOMVP9 includes a HOM3040M200TC load center, which will accept a maximum of 10 tandem breakers.
NOTE: The HOMVP9 is obsolete and no longer offered. 

CTA-ID : 15083
Was this helpful?
What can we do to improve the information ?