Technical FAQs

Ask a Question

What is the difference between the catalog numbers HOM3040M200TC and HOM3040M200TCK?

Issue:
Product Design Features

Product Line:
Homeline load centers

Resolution:
The "K" suffix in the catalog number indicated the load center was equipped with the "WireGator" feature for securing Romex cable.

NOTE: Both of these load centers are OBSOLETE and REPLACED BY THE CURRENT Plug-ON Neutral Design. SEE THE CURRENT SE DIGEST FOR CATALOG NUMBERS

CTA-ID : 15327
Was this helpful?
What can we do to improve the information ?