Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H82254 Double Throw Safety Switch?

The lugs on this device will accept (1) #6 AWG - 300 kcmil Aluminum or Copper conductors per phase.


CTA-ID : 15591
Was this helpful?
What can we do to improve the information ?