Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 82254 Double Throw Safety Switch?

Issue:
Product design features

Product Line:
Double Throw Safety Swithces

Environment:
Main lug wire sizes

Cause:
Application

Resolution:
The lugs on this device will accept (1) #6 AWG - 300 kcmil Aluminum or Copper conductors per phase. There are NO alternate lugs for this switch.


CTA-ID : 15587
Was this helpful?
What can we do to improve the information ?