Technical FAQs

Ask a Question

Does the QO13040M200 load center have copper bus?

Issue:
Confirming if the load center is provided with copper bus

Product Line:

QO and Homeline Load Centers

Environment:
Determining what material is used for the bus bars

Cause:
Meet specifications

Resolution:
Yes, this load center uses tin plated copper bus.


CTA-ID : 14583
Was this helpful?
What can we do to improve the information ?