Technical FAQs

Ask a Question

What quantity and size of conductors will a PK15GTAL ground bar accept?

This equipment ground kit has 15 terminals and each terminal will accept (1) #14 - #4 or (2) #14 - #12 copper conductors, or (1) #12 - #4 or (2) #12 - #10 aluminum conductors. There is also one lug terminal capable of terminating (1) #1 - #4/0 copper or aluminum conductor. The ground bar is 8.13 inches long .


CTA-ID : 14577
Was this helpful?
What can we do to improve the information ?