Technical FAQs

Ask a Question

What are the repair parts for a Q2E2200NRBCP, Series E03 Enclosed Circuit Breaker?

Only the parts listed below are considered field replaceable.
Circuit Breaker - Q2L2200 (Obsolete - replace with QBL22200)
Cover - 4050577001
Cover Mounting Screw - (2) 2142717161    
Interior Trim - 4050578201
Interior Trim Mounting Screw - 4020513001K
Neutral Assembly - 4051520151
Neutral Assembly Mounting Screw - (2) 2190320160
Neutral Bonding Screw - 4028318578      
NOTE: Covers and Interior Trims do not have labels applied.


CTA-ID : 14399
Was this helpful?
What can we do to improve the information ?