Technical FAQs

Ask a Question

Please ID the following part number XU2P18PD9AB?<br />

Its special for Chrysler that uses a std XU2P18PP340 sensor with a M12 connector pre-wired dark mode.

This modified special replaces an obsolete standard product that was specifically light or dark operated.

XU2P18PD9ABW is the same deal as above except with a 90 degree head.

CTA-ID : 14389
Was this helpful?
What can we do to improve the information ?