Technical FAQs

Ask a Question

What is the acceptable wire size range for the 9421ND* door mounted disconnect switch?

#14 to #4 AWG 60 or 75 degree C copper wire only, required terminal toque is 35 lbs./in.



CTA-ID : 14559
Was this helpful?
What can we do to improve the information ?