Technical FAQs

Ask a Question

What is the acceptable wire size range for the 9421NC* door mounted disconnect switch?

#14 to #8 AWG 75 degree C copper wire only, required terminal torque is 12 lbs./in.


CTA-ID : 14558
Was this helpful?
What can we do to improve the information ?