Technical FAQs

Ask a Question

Which standards does the Masterpact NT Insulated Case Circuit Breaker (Drawout and Fixed) meet?

UL489
NEMA AB1
CSA C22.2 No. 5.1 (CSA Certified)


CTA-ID : 14372
Was this helpful?
What can we do to improve the information ?