Technical FAQs

Ask a Question

Which standards does the Masterpact NT Drawout Low-voltage Power Circuit Breaker meet?<br />

ANSI C37.13
ANSI C37.16
ANSI C37.17
ANSI C37.50
UL1066 (cUL)
CSA C22.2 No. 31 (cUL)
NMX J-266-ANCE
NEMA SG3


CTA-ID : 14371
Was this helpful?
What can we do to improve the information ?