Technical FAQs

Ask a Question

Was there ever a QOD breaker, 3 phase breaker, two outer poles plug into panel, center pole has lugs on both ends.

Yes, QO delta breaker. NLA. This was used to plug into a single phase panel and feed a 3 phase load. Customer would terminate the 3rd phase on the line side lug of breaker to get the 3rd phase. Suggest 3 phase panel.


CTA-ID : 14140
Was this helpful?
What can we do to improve the information ?