Technical FAQs

Ask a Question

Do we offer a pigtail or M12 micro connector for the XCMA mini limit switches?

Add suffix T200= 5 pin micro
T300= 4 pin micro
L0120= 0.8meter cable with M12 pig tail.
M1020= 0.8 meter cable with 7/8 inch mini pig tail.

CTA-ID : 14138
Was this helpful?
What can we do to improve the information ?