Technical FAQs

Ask a Question

What are the features of the Micrologic 6.0P Trip Unit?

1--Indication of tripping cause
2--High resolution screen
3--Measurement display
4--Navigation buttons
5--Long-time current setting and tripping delay
6--Short-time pickup and tripping delay
7--Hole for settings lockout pin
8--Ground-fault pickup and tripping delay
9--Test lamp and indication reset
10--Maintenance indicators
11--Protection settings
12--Overload signal (LED)
13--Long-time rating plug screw
14--Instantaneous pickup
15--Electronic push-to-trip
16--Test connector


CTA-ID : 14557
Was this helpful?
What can we do to improve the information ?