Technical FAQs

Ask a Question

What are the features of the Micrologic 6.0A Trip Unit?

1--Indication of tripping cause
2--Navigation buttons
3--Long-time current setting and tripping delay
4--Short-time pickup and tripping delay
5--Ground-fault pickup and tripping delay
6--Test lamp and reset
7--Digital display
8--Three-phase bar graph and ammeter
9--Overload signal (LED)
10--Long-time rating plug screw
11--Instantaneous pickup
12--Electronic push-to-trip
13--Test connector


CTA-ID : 14556
Was this helpful?
What can we do to improve the information ?