Technical FAQs

Ask a Question

What are the features of the Micrologic 5.0 Basic Trip Unit?

1--Long-time current setting and tripping delay
2--Short-time pickup and tripping delay
3--Overload signal (LED)
4--Long-time rating plug screw
5--Instantaneous pickup
6--Test connector


CTA-ID : 14555
Was this helpful?
What can we do to improve the information ?