Technical FAQs

Ask a Question

Is the MA1000F enclosure available with a stainless steel cover?

Yes, we do offer a MA1000FSS, which would be supplied with a Type 304 stainless steel front cover. The device is not UL Listed and a minimum quantity of 10 is required.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 14553
Was this helpful?
What can we do to improve the information ?