Technical FAQs

Ask a Question

Is the FA100F enclosure available with a stainless steel cover?

Yes, we do offer a FA100FSS, which would be supplied with a Type 304 stainless steel front cover. The device is not UL Listed and a minimum quantity of 10 is required.


CTA-ID : 14546
Was this helpful?
What can we do to improve the information ?