Technical FAQs

Ask a Question

Is a flush cover available to replace the surface cover of a QO48M60DSGP generator panel?

A flush cover, part number 4055310750 (obsolete and replaced by 4055345250), will physically fit on the device, but will also require mounting screws, part number 4020513002K, to be purchased separately. No labels or stickers are included with the cover.

CTA-ID : 14365
Was this helpful?
What can we do to improve the information ?