Technical FAQs

Ask a Question

Is a NEMA 4, NEMA 4X or NEMA 5 stainless steel enclosure available for a NAL, NCL or NXL circuit breaker?

The only individually mounted enclosure available for the NAL, NCL or NXL circuit breaker is the NA1200AWK. It is rated for use in NEMA 3R, NEMA 3S or NEMA 12 applications.



CTA-ID : 14776
Was this helpful?
What can we do to improve the information ?