Technical FAQs

Ask a Question

How does a 9034 LLV80 operate.

The stem of the switch is a magnetically actuated reed switch. The float, containing a small magnet mounted off center, moves on the stem. It can be set for contacts to open on liquid rise, or close on liquid rise. The customer supplied conduit that screws into the stem of the switch serves as the mounting hardware. The low wattage of this unit requires the use of interposing relays in most cases.


CTA-ID : 14767
Was this helpful?
What can we do to improve the information ?