Technical FAQs

Ask a Question

What are the replacement parts for a HOMC42UC, Series S01, load center cover?

Issue:
Current design repair parts

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field repairable parts:
Door Hinge - 4028356450K (3 Req`d)
Door Latch and Spring - 4020284450K
Cover Mounting Screw - 4020513002K (10 Pack)
Directory Label - LSDL (This is a generic 1-42 circuit label)


CTA-ID : 14355
Was this helpful?
What can we do to improve the information ?