Technical FAQs

Ask a Question

Are the inputs and outputs isolated on the ATV28 drive?

Issue:  Are the inputs and outputs isolated on the ATV28 drive?
 
Product Line:  ATV28
 
Environment:  All
 
Cause:  N/A
 
Resolution:  All the inputs and outputs go to the microprocessor which comprises the control section.
The control section is galvanically isolated from the power section.


 
Was this helpful?
What can we do to improve the information ?