Technical FAQs

Ask a Question

What are the repair parts for the H362AWC, series F3 (may be shown as F03)?

Previous Design Repair Parts

Product Line:
Heavy Duty Safety Switches

Repair parts


The repair parts for the H362AWC, series F3 (F03) are as follows. No other parts are available.
-Line Base Assembly -4056614850 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 4056614451 (requires one per switch)
-Line and Load Base Mounting Screw - 4020515101(3 for line & 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR0306FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL0306F (one kit includes all line and load lugs)
-Receptacle - 2541002311
-Receptacle Mounting Screws - 4510280101 (required 4)

CTA-ID : 14758
Was this helpful?
What can we do to improve the information ?