Technical FAQs

Ask a Question

Does Square D offer NEMA 3R rated instrument transformers?<br /><or><br />Are the Digest listed current and potential transformers suitable for outdoor installation?

Square D instrument transformers are rated for indoor use only. As such, these devices should be protected from the elements in a suitable enclosure.

CTA-ID : 14520
Was this helpful?
What can we do to improve the information ?