Technical FAQs

Ask a Question

Is there a piece of EZM metering mounting channel available that could be cut to any desired length in the field?<br />

There is a 6` (6 foot) piece of EZM mounting channel available. It can be cut in the field to meet specific length requirements. The catalog number is EZM72MC.

CTA-ID : 14517
Was this helpful?
What can we do to improve the information ?