Technical FAQs

Ask a Question

Can the ATV28 drive accept 4-20 mA analog input?

Issue:   Can the ATV28 drive accept 4-20 mA analog input?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Yes. It can be used as a summed reference, speed reference or PI regulator feedback. It can also be configured as a 0-20mA current loop. The input is located at terminal AIC.


 
Was this helpful?
What can we do to improve the information ?