Technical FAQs

Ask a Question

What are the repair parts for a H225XKA Enclosed Molded Case Switch?

Only the parts listed below are considered field replaceable.
Molded Case Switch - KHL36000M
External Operating Handle - CBHK100H
Threaded Bushing - YOKK8747
Individual covers on Hazardous Location equipment cannot be supplied since the cover and enclosures are milled to match together. A damaged cover or enclosure will require a complete new device be used.

CTA-ID : 14515
Was this helpful?
What can we do to improve the information ?