Technical FAQs

Ask a Question

What are the repair parts for a H100XFA1212 Enclosed Molded Case Switch?

Only the parts listed below are considered field replaceable.
Molded Case Switch - FHL36000M1212
External Operating Handle - CBHK100H
Threaded Bushing - YOKK8206
Individual covers on Hazardous Location equipment cannot be supplied since the cover and enclosures are milled to match together. A damaged cover or enclosure will require a complete new device be used.


CTA-ID : 14514
Was this helpful?
What can we do to improve the information ?