Technical FAQs

Ask a Question

What are the repair parts for the H362AWA, series F1 (may be shown as F01)?

The repair parts for the H362AWA, series F1 (F01) are as follows. No other parts are available.
-Line Base Assembly -4056720850 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 4056614451 (requires one per switch)
-Line and Load Base Mounting Screw - 4020515101(3 for line & 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR0306FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL0306F (one kit includes all line and load lugs)
-Receptacle - WRDK6034
-Receptacle Mounting Screws - 4510280101 (required 4)

CTA-ID : 14752
Was this helpful?
What can we do to improve the information ?