Technical FAQs

Ask a Question

What are the repair parts for the H361AWA, series F3 (may be shown as F03)?

The repair parts for the H361AWA, series F3 (F03) are as follows. No other parts are available.
-Line Base Assembly -40566-147-50 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 40566-143-50 (requires one per switch)
-Line and Load Base Mounting Screw - 40205-151-01(3 for line & 2 for load)
-Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
-Arc Suppressor Mounting Screw - 40205-145-01
-Handle/Mechanism kit - HMR0306FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL0306F (one kit includes all line and load lugs)
-Receptacle - WRDK3034
-Receptacle Mounting Screws - 45102-801-01 (required 4)


CTA-ID : 14745
Was this helpful?
What can we do to improve the information ?