Technical FAQs

Ask a Question

We are installing AL250KA lugs on a KHL36150 breaker . But the breaker pad is threaded as well as the lugs. They will not tighten up?

You have to remove the termination inset on the bottom of lug pad on the breaker.
The screw goes thru the termnal pad and is tightened up by the threaded lug.


CTA-ID : 14074
Was this helpful?
What can we do to improve the information ?