Technical FAQs

Ask a Question

OBSOLETE - (See FA87450) What is the catalog number for a 50 ampere, 2 pole, GFCI Trilliant branch breaker?

Issue:
What is the catalog number for a 50 ampere, 2 pole, GFCI Trilliant branch breaker?

Product Line:
Trilliant model Miniature Circuit Breakers

Environment:
These breakers are only for the Trilliant style load center.

Cause:
The Trilliant load center and breakers are obsolete. Some breakers are still available until they run out of stock.

Resolution:
This is not available. We only offered GFCI branch breakers for Trilliant panels in 15 ampere, 1 pole (SDT115GFI) and 20 ampere, 1 pole (SDT120GFI). The SDT115GFI and SDT120GFI are now obsolete and no longer available. Contact your local qualified electrician for options.


CTA-ID : 14488
Was this helpful?
What can we do to improve the information ?