Technical FAQs

Ask a Question

What is the Equipment Ground Kit for H223DS, safety switch?

The Equipment Ground Kit is factory installed in this switch (F design series). Two ground lugs are provided, each accepting (1) #12 - 1/0 aluminum or (1) #14 - 1/0 copper ground conductor.

CTA-ID : 14315
Was this helpful?
What can we do to improve the information ?