Technical FAQs

Ask a Question

What type of hubs are used with the MPR22125 Meter-Pak?

This Meter-Paks` utility compartment will accept an A type hub (1`` through 2.5``) in the top endwall. Closing Plate ACP is factory installed on the top endwall for a bottom cable entry application. The bottom endwall will accept an A type hub (1`` through 2.5``) or a B300 (3`` hub).


CTA-ID : 14059
Was this helpful?
What can we do to improve the information ?