Technical FAQs

Ask a Question

What frequency range (bandwidth) can the SDM38VBIR Video Amplifier Hub be applied on?

Published specifications are 54 - 806 MHz. However, Square D can self-certify that the maximum frequency be extended to 1,000 MHz (1 GHz).

CTA-ID : 14048
Was this helpful?
What can we do to improve the information ?