Technical FAQs

Ask a Question

DUPLICATE SEE FA96493 - Does the QO342M150 load center have copper bus?

THIS IS A DUPLICATE SEE FA96493

Yes, this load center uses tin plated copper bus.


CTA-ID : 14722
Was this helpful?
What can we do to improve the information ?