Technical FAQs

Ask a Question

Does the QO330M150 load center have copper bus?

Issue:
Does the QO330M150 load center have copper bus?

Product Line:
QO and Homeline Load Centers

Environment:

Determining what material is used for the bus bars

Cause:

Meet specifications

Resolution:

Yes, this load center uses tin plated copper bus.


CTA-ID : 14721
Was this helpful?
What can we do to improve the information ?