Technical FAQs

Ask a Question

Does the QO330M125 load center have copper bus?

Issue:
Does the QO330M125 load center have copper bus?

Product Line:

QO and Homeline Load Centers

Environment:
Determining what material is used for the bus bars

Cause:
Meet specifications

Resolution:

Yes, this load center uses tin plated copper bus.


CTA-ID : 14720
Was this helpful?
What can we do to improve the information ?