Technical FAQs

Ask a Question

Are the different Main Control Boards for the entire line of ATV66 Drives interchangeable? For example, can I use VX4A66CK2 control kit on drive that normally uses VX4A66CK1?

No. The proper Main Control Board must be used with each drive.

** attached is link to receiving, installation, start-up manual which has spare parts list in the appendix with drives and corresponding control basket part #s **

CTA-ID : 14293
Was this helpful?
What can we do to improve the information ?