Technical FAQs

Ask a Question

How can an Altivar 58 drive be run using keypad command?

Enter into menu 4 (Control Menu). Scroll down to LCC (Keypad Com). Set to yes.
If using any stop types on any Logic input that input must have 24 VDC for the drive to run.
When the run button is pressed the drive will start at the low speed (LSP) until speed is increased by changing the frequency reference (LFr) in the display or adjust menus.
See keypad display user`s guide (VVDED397047US) for additional details.

CTA-ID : 14289
Was this helpful?
What can we do to improve the information ?