Technical FAQs

Ask a Question

What type of material is the H225XKA enclosure manufactured from?

This enclosure is manufactured from cast aluminum. It is considered to be copper free (less than .004% copper) in content.


CTA-ID : 14040
Was this helpful?
What can we do to improve the information ?