Technical FAQs

Ask a Question

Does the QO140M200K load center have copper bus?

Issue:
Confirming if the load center is provided with copper bus

Product Line:
QO and Homeline Load Centers

Environment:

Determining what material is used for the bus bars

Cause:
Meet specifications

Resolution:

Yes, this load center uses tin plated copper bus.


CTA-ID : 14706
Was this helpful?
What can we do to improve the information ?