Technical FAQs

Ask a Question

What are the repair parts for the H362AWA, series F5 (may be shown as F05)?

Issue:
Previous Design Repair Parts 

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The repair parts for the H362AWA, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly -4056720850 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 4056614451 (requires one per switch)
-Line and Load Base Mounting Screw - 4020515101(3 for line & 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR0306FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL0306F (one kit includes all line and load lugs)
-Receptacle - WRDK6034
-Receptacle Mounting Screws - 4510280101 (required 4)



CTA-ID : 14467
Was this helpful?
What can we do to improve the information ?